Motor_Start_Delay_Pulses
Motor_Start_Delay_Pulses
| Address: | 8764 (223CH) |
| Type: | WORD |
| Access: | Read/Write |
| Unit: | Pulses |
| Range: | 0 to 65535 |
| Default Value: | 0 |
| Store Supported: | Yes |
| Description: |
It defines the delay on the motor start expressed in pulses received from Counter #1. This object is generally used when electric gear feature is enabled. This object can be used to have repetitive motor starts. Each time the motor has to start (MOVE command executed, or Motor_SYNC object written or Trigger Start input detected) Motor_Start_Delay_Pulses pulses are waited from Counter #1. |
| Notes: |
This object should not be used together with Motor_Start_Delay object. |